Show / Hide Table of Contents

Classes

AddDoubleConverter

Adds a double provided via the converter parameter to the value.

BitmapConverter

Implements methods to convert bitmap sources.

BooleanConverter<T>

Base class for converting boolean values.

BooleanMultiConverterExtension

Converts a few boolean values to one boolean value depending on the boolean operation

BooleanToVisibilityConverter

Implements bool to Visibility Visibility converter.

CalculateDoubleConverter

Converts an IConvertible by applying a calculation operation with a value provided by the ConverterParameter. Or applies the calculation operation to every value when used as IMultiValueConverter.

ColorToBrushConverter

Converts given Color to SolidColorBrush

ConverterExtensionBase

Base class for value converter.

DoubleComparisonToBooleanConverter

Compares a double to the converter parameter and converts to a boolean. If used as IMultiValueConverter the first value is compared to the second.

EmptyEnumerableToVisibilityConverter

Converter an enumerable to Visibility.Collapsed

EmptyStringToVisibilityConverter

Converts an string to Visibility. If the string is null or empty the Null value is returned.

FlagEnumToBooleanConverter

Converts an enumeration to a boolean if the given enum value has the flag provided by the converter parameter.

FormattingConverter

Converts multi values according to a bound format string.

HasIDataErrorInfoToBooleanConverter

Checks whether the value to convert implements IDataErrorInfo.

InverseBooleanConverter

Inverse convertion of a boolean

IsTypeConverter

Converts an object to a Boolean. Yields True if the object is of the Type provided by the converter parameter.

MarkdownLinkConverter

Converts a string containing markdown style links to a TextBlock.

MultiBooleanToVisibilityConverterExtension

Converts a few boolean values to a Visibility value depending on the boolean operation

MultiConverterExtensionBase

Base class for MultiValueConverter

NullConverter<T>

Implements an abstract null converter.

NullOrEmptyConverter<T, TResult>

Implements an abstract null or empty converter.

NullToBooleanConverter

Converts a value to true if it is not null, otherwise to false.

NullToVisibilityConverter

Converts a value to Visible if it is not null, otherwise to Collapsed.

PanelWidthConverter

Converts the ActualWidth of the Parent window to the width of the "FilterControl".

PopupWidthConverter

StringIsNullOrEmptyToBooleanConverter

Converts a string to a boolean depending whether the string is null or empty

StringToResourceConverter

Get a Resource by Key

ThicknessMultiConverter

This converter takes values and converts them to a Thickness:

ToUpperStringConverter

Converts a string to upper case.

TreeViewItemDepthToIndentionConverter

Converts to the correct left margin for a TreeViewItem based on its level depth in the TreeView.

ValidationSeverityToVisibilityConverter

Convert ValidationSeverity to visibility.

VisibilityToBooleanConverter

Converts the Visibility to a bool where Visible equals true and Collapsed equals false.

VisibilityToGridLengthConverter

converts visibility property to * or Auto

Enums

BoolOperation

Defines boolean operations

CalcOperation

Defines a calculation operation

ComparisonType

The type of comparison used in the DoubleComparisonToBooleanConverter

Back to top Generated by DocFX