Show / Hide Table of Contents

Class FormattingConverter

Converts multi values according to a bound format string.

Inheritance
object
FormattingConverter
Implements
IMultiValueConverter
object.Equals(object)
object.Equals(object, object)
object.GetHashCode()
object.GetType()
object.MemberwiseClone()
object.ReferenceEquals(object, object)
object.ToString()
Namespace: Sartorius.SAF.Presentation.Converter
Assembly: Sartorius.SAF.Presentation.dll
Syntax
public class FormattingConverter : IMultiValueConverter
Remarks

Uses the last value provided as formatted string.

Examples
<ContentControl Focusable="False"
        IsTabStop="False"
        VerticalAlignment="Center"
        FontFamily="{DynamicResource SAF_Font_Base_Arial}"
        FontSize="12"
        Foreground="{DynamicResource SAF_FG_S07}">
    <ContentControl.Content>
        <MultiBinding>
            <Binding RelativeSource="{RelativeSource TemplatedParent}" Path="SelectedItemsView.Count" />
            <Binding RelativeSource="{RelativeSource TemplatedParent}" Path="MaxSelectedItemCount" />
            <Binding RelativeSource="{RelativeSource TemplatedParent}" Path="SelectionCountFormat" />
        </MultiBinding>
    </ContentControl.Content>
</ContentControl>

Methods

View Source

Convert(object[], Type, object, CultureInfo)

Converts source values to a value for the binding target. The data binding engine calls this method when it propagates the values from source bindings to the binding target.

Declaration
public object Convert(object[] values, Type targetType, object parameter, CultureInfo culture)
Parameters
Type Name Description
object[] values

The array of values that the source bindings in the MultiBinding produces. The value UnsetValue indicates that the source binding has no value to provide for conversion.

Type targetType

The type of the binding target property.

object parameter

The converter parameter to use.

CultureInfo culture

The culture to use in the converter.

Returns
Type Description
object

A converted value.If the method returns null, the valid null value is used.A return value of DependencyProperty.UnsetValue indicates that the converter did not produce a value, and that the binding will use the FallbackValue if it is available, or else will use the default value.A return value of Binding.DoNothing indicates that the binding does not transfer the value or use the FallbackValue or the default value.

View Source

ConvertBack(object, Type[], object, CultureInfo)

Converts a binding target value to the source binding values.

Declaration
public object[] ConvertBack(object value, Type[] targetTypes, object parameter, CultureInfo culture)
Parameters
Type Name Description
object value

The value that the binding target produces.

Type[] targetTypes

The array of types to convert to. The array length indicates the number and types of values that are suggested for the method to return.

object parameter

The converter parameter to use.

CultureInfo culture

The culture to use in the converter.

Returns
Type Description
object[]

An array of values that have been converted from the target value back to the source values.

Implements

IMultiValueConverter

Extension Methods

CollectionExtensions.AddRange<T, TCollection>(TCollection, IEnumerable<T>)
SerializableObjectCloneExtension.Clone<T>(T)
  • View Source
Back to top Generated by DocFX