Show / Hide Table of Contents

Class CalculateDoubleConverter

Converts an IConvertible by applying a calculation operation with a value provided by the ConverterParameter. Or applies the calculation operation to every value when used as IMultiValueConverter.

Inheritance
object
CalculateDoubleConverter
Implements
IValueConverter
IMultiValueConverter
object.Equals(object)
object.Equals(object, object)
object.GetHashCode()
object.GetType()
object.MemberwiseClone()
object.ReferenceEquals(object, object)
object.ToString()
Namespace: Sartorius.SAF.Presentation.Converter
Assembly: Sartorius.SAF.Presentation.dll
Syntax
public class CalculateDoubleConverter : IValueConverter, IMultiValueConverter
Remarks

Values and parameters provided to this converter must be IConvertible. If any value or parameter is not IConvertible 1 will be assumed as its value.

The converter can ConvertBack(object, Type, object, CultureInfo) if used as IValueConverter. As IMultiValueConverter ConvertBack(object, Type[], object, CultureInfo) is not possible. It will throw an NotSupportedException.

Properties

View Source

Operation

Gets or sets the operation that should be applied to values.

Declaration
public CalcOperation Operation { get; set; }
Property Value
Type Description
CalcOperation

The operation.

Methods

View Source

Convert(object, Type, object, CultureInfo)

Converts a value.

Declaration
public object Convert(object value, Type targetType, object parameter, CultureInfo culture)
Parameters
Type Name Description
object value

The value produced by the binding source.

Type targetType

The type of the binding target property.

object parameter

The converter parameter to use.

CultureInfo culture

The culture to use in the converter.

Returns
Type Description
object

A converted value. If the method returns null, the valid null value is used.

View Source

Convert(object[], Type, object, CultureInfo)

Converts source values to a value for the binding target. The data binding engine calls this method when it propagates the values from source bindings to the binding target.

Declaration
public object Convert(object[] values, Type targetType, object parameter, CultureInfo culture)
Parameters
Type Name Description
object[] values

The array of values that the source bindings in the MultiBinding produces. The value UnsetValue indicates that the source binding has no value to provide for conversion.

Type targetType

The type of the binding target property.

object parameter

The converter parameter to use.

CultureInfo culture

The culture to use in the converter.

Returns
Type Description
object

A converted value.If the method returns null, the valid null value is used.A return value of DependencyProperty.UnsetValue indicates that the converter did not produce a value, and that the binding will use the FallbackValue if it is available, or else will use the default value.A return value of Binding.DoNothing indicates that the binding does not transfer the value or use the FallbackValue or the default value.

View Source

ConvertBack(object, Type, object, CultureInfo)

Converts a value.

Declaration
public object ConvertBack(object value, Type targetType, object parameter, CultureInfo culture)
Parameters
Type Name Description
object value

The value that is produced by the binding target.

Type targetType

The type to convert to.

object parameter

The converter parameter to use.

CultureInfo culture

The culture to use in the converter.

Returns
Type Description
object

A converted value. If the method returns null, the valid null value is used.

View Source

ConvertBack(object, Type[], object, CultureInfo)

Converts a binding target value to the source binding values.

Declaration
public object[] ConvertBack(object value, Type[] targetTypes, object parameter, CultureInfo culture)
Parameters
Type Name Description
object value

The value that the binding target produces.

Type[] targetTypes

The array of types to convert to. The array length indicates the number and types of values that are suggested for the method to return.

object parameter

The converter parameter to use.

CultureInfo culture

The culture to use in the converter.

Returns
Type Description
object[]

An array of values that have been converted from the target value back to the source values.

Implements

IValueConverter
IMultiValueConverter

Extension Methods

CollectionExtensions.AddRange<T, TCollection>(TCollection, IEnumerable<T>)
SerializableObjectCloneExtension.Clone<T>(T)
  • View Source
Back to top Generated by DocFX