Show / Hide Table of Contents

Class VisibilityToBooleanConverter

Converts the Visibility to a bool where Visible equals true and Collapsed equals false.

Inheritance
object
VisibilityToBooleanConverter
Implements
IValueConverter
object.Equals(object)
object.Equals(object, object)
object.GetHashCode()
object.GetType()
object.MemberwiseClone()
object.ReferenceEquals(object, object)
object.ToString()
Namespace: Sartorius.SAF.Presentation.Converter
Assembly: Sartorius.SAF.Presentation.dll
Syntax
public class VisibilityToBooleanConverter : IValueConverter

Constructors

View Source

VisibilityToBooleanConverter()

constructor for VisibilityToBooleanConverter, sets default Visible to true. Incoming Visibility is != Visibility.Visible returns false

Declaration
public VisibilityToBooleanConverter()

Properties

View Source

Visible

Gets or sets the bool that is returned when the Visibility is Visible. Incoming Visibility is != Visibility.Visible returns !Visible, Default: true

Declaration
public bool Visible { get; set; }
Property Value
Type Description
bool

Methods

View Source

Convert(object, Type, object, CultureInfo)

Converts a value.

Declaration
public object Convert(object value, Type targetType, object parameter, CultureInfo culture)
Parameters
Type Name Description
object value

The value produced by the binding source.

Type targetType

The type of the binding target property.

object parameter

The converter parameter to use.

CultureInfo culture

The culture to use in the converter.

Returns
Type Description
object

A converted value. If the method returns null, the valid null value is used.

View Source

ConvertBack(object, Type, object, CultureInfo)

Converts a value.

Declaration
public object ConvertBack(object value, Type targetType, object parameter, CultureInfo culture)
Parameters
Type Name Description
object value

The value that is produced by the binding target.

Type targetType

The type to convert to.

object parameter

The converter parameter to use.

CultureInfo culture

The culture to use in the converter.

Returns
Type Description
object

A converted value. If the method returns null, the valid null value is used.

Implements

IValueConverter

Extension Methods

CollectionExtensions.AddRange<T, TCollection>(TCollection, IEnumerable<T>)
SerializableObjectCloneExtension.Clone<T>(T)
  • View Source
Back to top Generated by DocFX