Show / Hide Table of Contents

Class ConverterExtensionBase

Base class for value converter.

Inheritance
object
MarkupExtension
ConverterExtensionBase
BrushToColorConverter
ColorToStrokeConverter
ThumbWidthToMarginConverter
BooleanConverter<T>
ColorToBrushConverter
IsTypeConverter
MarkdownLinkConverter
NullConverter<T>
Implements
IValueConverter
object.Equals(object)
object.Equals(object, object)
object.GetHashCode()
object.GetType()
object.MemberwiseClone()
object.ReferenceEquals(object, object)
object.ToString()
Namespace: Sartorius.SAF.Presentation.Converter
Assembly: Sartorius.SAF.Presentation.dll
Syntax
public class ConverterExtensionBase : MarkupExtension, IValueConverter

Methods

View Source

Convert(object, Type, object, CultureInfo)

Converts a value.

Declaration
public virtual object Convert(object value, Type targetType, object parameter, CultureInfo culture)
Parameters
Type Name Description
object value

The value produced by the binding source.

Type targetType

The type of the binding target property.

object parameter

The converter parameter to use.

CultureInfo culture

The culture to use in the converter.

Returns
Type Description
object

A converted value. If the method returns null, the valid null value is used.

View Source

ConvertBack(object, Type, object, CultureInfo)

Converts a value.

Declaration
public virtual object ConvertBack(object value, Type targetType, object parameter, CultureInfo culture)
Parameters
Type Name Description
object value

The value that is produced by the binding target.

Type targetType

The type to convert to.

object parameter

The converter parameter to use.

CultureInfo culture

The culture to use in the converter.

Returns
Type Description
object

A converted value. If the method returns null, the valid null value is used.

View Source

ProvideValue(IServiceProvider)

When implemented in a derived class, returns an object that is provided as the value of the target property for this markup extension.

Declaration
public override object ProvideValue(IServiceProvider serviceProvider)
Parameters
Type Name Description
IServiceProvider serviceProvider

A service provider helper that can provide services for the markup extension.

Returns
Type Description
object

The object value to set on the property where the extension is applied.

Overrides
MarkupExtension.ProvideValue(IServiceProvider)

Implements

IValueConverter

Extension Methods

CollectionExtensions.AddRange<T, TCollection>(TCollection, IEnumerable<T>)
SerializableObjectCloneExtension.Clone<T>(T)
  • View Source
Back to top Generated by DocFX