Class EmptyEnumerableToVisibilityConverter
Converter an enumerable to Visibility.Collapsed
Implements
Namespace: Sartorius.SAF.Presentation.Converter
Assembly: Sartorius.SAF.Presentation.dll
Syntax
public class EmptyEnumerableToVisibilityConverter : IValueConverter
Constructors
View SourceEmptyEnumerableToVisibilityConverter()
Creates a new instance of the EmptyEnumerableToVisibilityConverter class.
Declaration
public EmptyEnumerableToVisibilityConverter()
Properties
View SourceEmpty
Gets or sets the Visibility that is returned when the IEnumerable is empty.
Declaration
public Visibility Empty { get; set; }
Property Value
| Type | Description |
|---|---|
| Visibility |
Filled
Gets or sets the Visibility that is returned when the IEnumerable is filled.
Declaration
public Visibility Filled { get; set; }
Property Value
| Type | Description |
|---|---|
| Visibility |
Methods
View SourceConvert(object, Type, object, CultureInfo)
Converts a value.
Declaration
public object Convert(object value, Type targetType, object parameter, CultureInfo culture)
Parameters
| Type | Name | Description |
|---|---|---|
| object | value | The value produced by the binding source. |
| Type | targetType | The type of the binding target property. |
| object | parameter | The converter parameter to use. |
| CultureInfo | culture | The culture to use in the converter. |
Returns
| Type | Description |
|---|---|
| object | A converted value. If the method returns null, the valid null value is used. |
ConvertBack(object, Type, object, CultureInfo)
Converts a value.
Declaration
public object ConvertBack(object value, Type targetType, object parameter, CultureInfo culture)
Parameters
| Type | Name | Description |
|---|---|---|
| object | value | The value that is produced by the binding target. |
| Type | targetType | The type to convert to. |
| object | parameter | The converter parameter to use. |
| CultureInfo | culture | The culture to use in the converter. |
Returns
| Type | Description |
|---|---|
| object | A converted value. If the method returns null, the valid null value is used. |