Show / Hide Table of Contents

Class BooleanMultiConverterExtension

Converts a few boolean values to one boolean value depending on the boolean operation

Inheritance
object
MarkupExtension
MultiConverterExtensionBase
BooleanMultiConverterExtension
MultiBooleanToVisibilityConverterExtension
Implements
IMultiValueConverter
MultiConverterExtensionBase.ConvertBack(object, Type[], object, CultureInfo)
MultiConverterExtensionBase.ProvideValue(IServiceProvider)
object.Equals(object)
object.Equals(object, object)
object.GetHashCode()
object.GetType()
object.MemberwiseClone()
object.ReferenceEquals(object, object)
object.ToString()
Namespace: Sartorius.SAF.Presentation.Converter
Assembly: Sartorius.SAF.Presentation.dll
Syntax
public class BooleanMultiConverterExtension : MultiConverterExtensionBase, IMultiValueConverter

Properties

View Source

BoolOperation

Gets or sets the boolean operation

Declaration
public BoolOperation BoolOperation { get; set; }
Property Value
Type Description
BoolOperation

Methods

View Source

Convert(object[], Type, object, CultureInfo)

Converts source values to a value for the binding target. The data binding engine calls this method when it propagates the values from source bindings to the binding target.

Declaration
public override object Convert(object[] values, Type targetType, object parameter, CultureInfo culture)
Parameters
Type Name Description
object[] values

The array of values that the source bindings in the MultiBinding produces. The value UnsetValue indicates that the source binding has no value to provide for conversion.

Type targetType

The type of the binding target property.

object parameter

The converter parameter to use.

CultureInfo culture

The culture to use in the converter.

Returns
Type Description
object

A converted value.If the method returns null, the valid null value is used.A return value of DependencyProperty.UnsetValue indicates that the converter did not produce a value, and that the binding will use the FallbackValue if it is available, or else will use the default value.A return value of Binding.DoNothing indicates that the binding does not transfer the value or use the FallbackValue or the default value.

Overrides
MultiConverterExtensionBase.Convert(object[], Type, object, CultureInfo)

Implements

IMultiValueConverter

Extension Methods

CollectionExtensions.AddRange<T, TCollection>(TCollection, IEnumerable<T>)
SerializableObjectCloneExtension.Clone<T>(T)
  • View Source
Back to top Generated by DocFX