Show / Hide Table of Contents

Class ToUpperStringConverter

Converts a string to upper case.

Inheritance
object
ToUpperStringConverter
Implements
IValueConverter
object.Equals(object)
object.Equals(object, object)
object.GetHashCode()
object.GetType()
object.MemberwiseClone()
object.ReferenceEquals(object, object)
object.ToString()
Namespace: Sartorius.SAF.Presentation.Converter
Assembly: Sartorius.SAF.Presentation.dll
Syntax
public class ToUpperStringConverter : IValueConverter

Methods

View Source

Convert(object, Type, object, CultureInfo)

Converts a value.

Declaration
public object Convert(object value, Type targetType, object parameter, CultureInfo culture)
Parameters
Type Name Description
object value

The value produced by the binding source.

Type targetType

The type of the binding target property.

object parameter

The converter parameter to use.

CultureInfo culture

The culture to use in the converter.

Returns
Type Description
object

A converted value. If the method returns null, the valid null value is used.

View Source

ConvertBack(object, Type, object, CultureInfo)

Converts a value.

Declaration
public object ConvertBack(object value, Type targetType, object parameter, CultureInfo culture)
Parameters
Type Name Description
object value

The value that is produced by the binding target.

Type targetType

The type to convert to.

object parameter

The converter parameter to use.

CultureInfo culture

The culture to use in the converter.

Returns
Type Description
object

A converted value. If the method returns null, the valid null value is used.

Implements

IValueConverter

Extension Methods

CollectionExtensions.AddRange<T, TCollection>(TCollection, IEnumerable<T>)
SerializableObjectCloneExtension.Clone<T>(T)
  • View Source
Back to top Generated by DocFX