Show / Hide Table of Contents

Classes

AssemblyResolver

Handles AppDomain's AssemblyResolve event to be able to load assemblies dynamically in the LoadFrom context, but be able to reference the type from assemblies loaded in the Load context.

CyclicDependencyFoundException

Represents the exception that is thrown when there is a circular dependency between modules during the module loading process.

DirectoryModuleCatalog

Represets a catalog created from a directory on disk.

DuplicateModuleException

Exception thrown when a module is declared twice in the same catalog.

FileModuleTypeLoader

Loads modules from an arbitrary location on the filesystem. This typeloader is only called if ModuleInfo classes have a Ref parameter that starts with "file://". This class is only used on the Desktop version of the Composite Application Library.

LoadModuleCompletedEventArgs

Provides completion information after a module is loaded, or fails to load.

ModularityException

Base class for exceptions that are thrown because of a problem with modules.

ModuleAttribute

Indicates that the class should be considered a named module using the provided module name.

ModuleCatalog

The ModuleCatalog holds information about the modules that can be used by the application. Each module is described in a ModuleInfo class, that records the name, type and location of the module. It also verifies that the ModuleCatalog is internally valid. That means that it does not have:

The ModuleCatalog also serves as a baseclass for more specialized Catalogs .

ModuleDependencyAttribute

Specifies that the current module has a dependency on another module. This attribute should be used on classes that implement IModule.

ModuleDependencySolver

Used by ModuleInitializer to get the load sequence for the modules to load according to their dependencies.

ModuleDownloadProgressChangedEventArgs

Provides progress information as a module downloads.

ModuleExportAttribute

Definition of attribute to export IModule via MEF.

ModuleInfo

Defines the metadata that describes a module.

ModuleInfoGroup

Represents a group of ModuleInfo instances that are usually deployed together. ModuleInfoGroups are also used by the ModuleCatalog to prevent common deployment problems such as having a module that's required at startup that depends on modules that will only be downloaded on demand. The group also forwards Ref and InitializationMode values to the ModuleInfos that it contains.

ModuleInfoGroupExtensions

Defines extension methods for the ModuleInfoGroup class.

ModuleInitializeException

Exception thrown by IModuleInitializer implementations whenever a module fails to load.

ModuleInitializer

Implements the IModuleInitializer interface. Handles loading of a module based on a type.

ModuleLocator

Locates modules of type IModule.

ModuleManager

Component responsible for coordinating the modules' type loading and module initialization process.

ModuleNotFoundException

Exception thrown when a requested OnDemand IModule was not found.

ModuleTypeLoaderNotFoundException

Base class for exceptions that are thrown because of a problem with modules.

ModuleTypeLoadingException

Exception thrown by IModuleManager implementations whenever a module fails to retrieve.

Interfaces

IAssemblyResolver

Interface for classes that are responsible for resolving and loading assembly files.

IModule

Definition of a module.

IModuleCatalog

This is the expected catalog definition for the ModuleManager. The ModuleCatalog holds information about the modules that can be used by the application. Each module is described in a ModuleInfo class, that records the name, type and location of the module.

IModuleCatalogItem

Marker interface that allows both ModuleInfoGroups and ModuleInfos to be added to the IModuleCatalog from code and XAML.

IModuleExport

Describe the Managed Extensibility Framework export of an IModule.

IModuleInitializer

Declares a service which initializes the modules into the application.

IModuleLocator

Defines a locator to locate modules of type IModule within the composition container.

IModuleManager

Defines the interface for the service that will retrieve and initialize the application's modules.

IModuleTypeLoader

Defines the interface for moduleTypeLoaders

Enums

InitializationMode

Specifies on which stage the Module group will be initialized.

ModuleProperties

Flags defining properties for a IModule

ModuleState

Defines the states a ModuleInfo can be in, with regards to the module loading and initialization process.

Back to top Generated by DocFX