Show / Hide Table of Contents

Interface IModuleManager

Defines the interface for the service that will retrieve and initialize the application's modules.

Namespace: Sartorius.SAF.Presentation.Modularity
Assembly: Sartorius.SAF.Presentation.dll
Syntax
public interface IModuleManager

Methods

View Source

LoadModule(string)

Loads and initializes the module on the ModuleCatalog with the name moduleName.

Declaration
void LoadModule(string moduleName)
Parameters
Type Name Description
string moduleName

Name of the module requested for initialization.

View Source

Run()

Initializes the modules marked as WhenAvailable on the ModuleCatalog.

Declaration
void Run()

Events

View Source

LoadModuleCompleted

Raised when a module is loaded or fails to load.

Declaration
event EventHandler<LoadModuleCompletedEventArgs> LoadModuleCompleted
Event Type
Type Description
EventHandler<LoadModuleCompletedEventArgs>
View Source

ModuleDownloadProgressChanged

Raised repeatedly to provide progress as modules are downloaded.

Declaration
event EventHandler<ModuleDownloadProgressChangedEventArgs> ModuleDownloadProgressChanged
Event Type
Type Description
EventHandler<ModuleDownloadProgressChangedEventArgs>

Extension Methods

CollectionExtensions.AddRange<T, TCollection>(TCollection, IEnumerable<T>)
SerializableObjectCloneExtension.Clone<T>(T)
  • View Source
Back to top Generated by DocFX