Class AssemblyResolver
Handles AppDomain's AssemblyResolve event to be able to load assemblies dynamically in the LoadFrom context, but be able to reference the type from assemblies loaded in the Load context.
Namespace: Sartorius.SAF.Presentation.Modularity
Assembly: Sartorius.SAF.Presentation.dll
Syntax
public class AssemblyResolver : IAssemblyResolver, IDisposable
Methods
View SourceDispose()
Performs application-defined tasks associated with freeing, releasing, or resetting unmanaged resources.
Declaration
public void Dispose()
Remarks
Calls Dispose(bool)
Dispose(bool)
Disposes the associated AssemblyResolver.
Declaration
protected virtual void Dispose(bool disposing)
Parameters
| Type | Name | Description |
|---|---|---|
| bool | disposing | When true, it is being called from the Dispose method. |
LoadAssemblyFrom(string)
Registers the specified assembly and resolves the types in it when the AppDomain requests for it.
Declaration
public void LoadAssemblyFrom(string assemblyFilePath)
Parameters
| Type | Name | Description |
|---|---|---|
| string | assemblyFilePath | The path to the assemly to load in the LoadFrom context. |
Remarks
This method does not load the assembly immediately, but lazily until someone requests a Type declared in the assembly.