Show / Hide Table of Contents

Class CyclicDependencyFoundException

Represents the exception that is thrown when there is a circular dependency between modules during the module loading process.

Inheritance
object
Exception
ModularityException
CyclicDependencyFoundException
Implements
ISerializable
ModularityException.ModuleName
Exception.GetBaseException()
Exception.GetType()
Exception.ToString()
Exception.Data
Exception.HelpLink
Exception.HResult
Exception.InnerException
Exception.Message
Exception.Source
Exception.StackTrace
Exception.TargetSite
Exception.SerializeObjectState
object.Equals(object)
object.Equals(object, object)
object.GetHashCode()
object.MemberwiseClone()
object.ReferenceEquals(object, object)
Namespace: Sartorius.SAF.Presentation.Modularity
Assembly: Sartorius.SAF.Presentation.dll
Syntax
public class CyclicDependencyFoundException : ModularityException, ISerializable

Constructors

View Source

CyclicDependencyFoundException()

Initializes a new instance of the CyclicDependencyFoundException class.

Declaration
public CyclicDependencyFoundException()
View Source

CyclicDependencyFoundException(string)

Initializes a new instance of the CyclicDependencyFoundException class with the specified error message.

Declaration
public CyclicDependencyFoundException(string message)
Parameters
Type Name Description
string message

The message that describes the error.

View Source

CyclicDependencyFoundException(string, Exception)

Initializes a new instance of the CyclicDependencyFoundException class with the specified error message and inner exception.

Declaration
public CyclicDependencyFoundException(string message, Exception innerException)
Parameters
Type Name Description
string message

The error message that explains the reason for the exception.

Exception innerException

The exception that is the cause of the current exception.

View Source

CyclicDependencyFoundException(string, string, Exception)

Initializes the exception with a particular module, error message and inner exception that happened.

Declaration
public CyclicDependencyFoundException(string moduleName, string message, Exception innerException)
Parameters
Type Name Description
string moduleName

The name of the module.

string message

The error message that explains the reason for the exception.

Exception innerException

The exception that is the cause of the current exception, or a null reference if no inner exception is specified.

Implements

ISerializable

Extension Methods

CollectionExtensions.AddRange<T, TCollection>(TCollection, IEnumerable<T>)
SerializableObjectCloneExtension.Clone<T>(T)
ExceptionExtensions.GetRootException(Exception)
  • View Source
Back to top Generated by DocFX