Interface IModuleTypeLoader
Defines the interface for moduleTypeLoaders
Namespace: Sartorius.SAF.Presentation.Modularity
Assembly: Sartorius.SAF.Presentation.dll
Syntax
public interface IModuleTypeLoader
Methods
View SourceCanLoadModuleType(ModuleInfo)
Evaluates the Ref property to see if the current typeloader will be able to retrieve the moduleInfo.
Declaration
bool CanLoadModuleType(ModuleInfo moduleInfo)
Parameters
| Type | Name | Description |
|---|---|---|
| ModuleInfo | moduleInfo | Module that should have it's type loaded. |
Returns
| Type | Description |
|---|---|
| bool | true if the current typeloader is able to retrieve the module, otherwise false. |
LoadModuleType(ModuleInfo)
Retrieves the moduleInfo.
Declaration
void LoadModuleType(ModuleInfo moduleInfo)
Parameters
| Type | Name | Description |
|---|---|---|
| ModuleInfo | moduleInfo | Module that should have it's type loaded. |
Events
View SourceLoadModuleCompleted
Raised when a module is loaded or fails to load.
Declaration
event EventHandler<LoadModuleCompletedEventArgs> LoadModuleCompleted
Event Type
| Type | Description |
|---|---|
| EventHandler<LoadModuleCompletedEventArgs> |
Remarks
This event is raised once per ModuleInfo instance requested in LoadModuleType(ModuleInfo).
ModuleDownloadProgressChanged
Raised repeatedly to provide progress as modules are downloaded in the background.
Declaration
event EventHandler<ModuleDownloadProgressChangedEventArgs> ModuleDownloadProgressChanged
Event Type
| Type | Description |
|---|---|
| EventHandler<ModuleDownloadProgressChangedEventArgs> |