Show / Hide Table of Contents

Class BrushToColorConverter

Converts a Brush into a Color.
Can only convert from SolidColorBrush or GradientBrush
Otherwise return value is DependencyProperty.UnsetValue

Inheritance
object
MarkupExtension
ConverterExtensionBase
BrushToColorConverter
Implements
IValueConverter
ConverterExtensionBase.ConvertBack(object, Type, object, CultureInfo)
ConverterExtensionBase.ProvideValue(IServiceProvider)
object.Equals(object)
object.Equals(object, object)
object.GetHashCode()
object.GetType()
object.MemberwiseClone()
object.ReferenceEquals(object, object)
object.ToString()
Namespace: Sartorius.SAF.Presentation.Controls
Assembly: Sartorius.SAF.Presentation.Controls.dll
Syntax
public class BrushToColorConverter : ConverterExtensionBase, IValueConverter

Methods

View Source

Convert(object, Type, object, CultureInfo)

Converts a value.

Declaration
public override object Convert(object value, Type targetType, object parameter, CultureInfo culture)
Parameters
Type Name Description
object value

The value produced by the binding source.

Type targetType

The type of the binding target property.

object parameter

The converter parameter to use.

CultureInfo culture

The culture to use in the converter.

Returns
Type Description
object

A converted value. If the method returns null, the valid null value is used.

Overrides
ConverterExtensionBase.Convert(object, Type, object, CultureInfo)

Implements

IValueConverter

Extension Methods

CollectionExtensions.AddRange<T, TCollection>(TCollection, IEnumerable<T>)
SerializableObjectCloneExtension.Clone<T>(T)
  • View Source
Back to top Generated by DocFX