Class ColorToStrokeConverter
Converts a Color to a stroke brush
Implements
Namespace: Sartorius.SAF.Presentation.Controls
Assembly: Sartorius.SAF.Presentation.Controls.dll
Syntax
public class ColorToStrokeConverter : ConverterExtensionBase, IValueConverter
Methods
View SourceConvert(object, Type, object, CultureInfo)
Converts a value.
Declaration
public override object Convert(object value, Type targetType, object parameter, CultureInfo culture)
Parameters
| Type | Name | Description |
|---|---|---|
| object | value | The value produced by the binding source. |
| Type | targetType | The type of the binding target property. |
| object | parameter | The converter parameter to use. |
| CultureInfo | culture | The culture to use in the converter. |
Returns
| Type | Description |
|---|---|
| object | A converted value. If the method returns null, the valid null value is used. |