Show / Hide Table of Contents

The Sartorius.SAF.Presentation.Behaviors namespace contains classes for reusable interactivity in SAF projects.

<Test></Test>

Classes

ComboBoxItemDisplayBehavior

Provides different ItemTemplates and/or an additional empty item for a ComboBox.

CommandBehaviorBase<T>

Base behavior to handle connecting a Control to a Command.

ContentPresenterTextTrimmingBehavior

Sets TextTrimming to CharacterEllipsis for the auto generated TextBlock of the ContentPresenter.

Interaction

Contains member for interaction between UI and code.

PasswordChangedBehavior

Defines a behavior for the PasswordBox password changed event.

PopupAutoCloseBehavior

Behavior that closes the Popup it is attached to after a delay

PopupPositioningBehavior

Behavior that positions the Popup relative to its PlacementTarget and within the borders of its Owner

SelectorCommandBehavior

Only for controls that are derived from Selector.

SettingBehavior<T>

Base class for all settings stored via xaml.

TextBoxClickCommandBehavior

Implements a command behavior for TextBox control.

TextBoxDecimalMaskingBehavior

Microsoft.Xaml.Behaviors.Behavior for masking a TextBox to allow only entering of decimal values.

TextBoxHexMaskingBehavior

see cref="Behavior"/> for masking a TextBox to allow only entering of hexadecimal values.

TextBoxIntMaskingBehavior

see cref="Behavior"/> for masking a TextBox to allow only entering of int values.

TextBoxMaskingBehaviorBase

Microsoft.Xaml.Behaviors.Behavior for masking a TextBox to allow only entering specific data.

TextChangedCommandBehavior

Implements a command behavior for TextBox control.

TreeViewBehavior

Implements a behaviors for tree view control.

TreeViewItemEventData

Implements the behavior event data.

ViewClosingBehavior

Implements a closing behavior for view.

WindowAltF4Behavior

Implements a behavior to supress the execution of 'windows Alt + F4' and optionally execute a command instead.

WindowDragMoveBehavior

Behavior for the activation of windows DragMove functionality.

Enums

TreeViewItemEventName

Defined a tree view item events.

  • Edit this page
Back to top Generated by DocFX