Show / Hide Table of Contents

Class TextChangedCommandBehavior

Implements a command behavior for TextBox control.

Inheritance
object
CommandBehaviorBase<TextBox>
TextChangedCommandBehavior
CommandBehaviorBase<TextBox>.Command
CommandBehaviorBase<TextBox>.CommandParameter
CommandBehaviorBase<TextBox>.TargetObject
CommandBehaviorBase<TextBox>.ExecuteCommand()
CommandBehaviorBase<TextBox>.UpdateEnabledState()
object.Equals(object)
object.Equals(object, object)
object.GetHashCode()
object.GetType()
object.MemberwiseClone()
object.ReferenceEquals(object, object)
object.ToString()
Namespace: Sartorius.SAF.Presentation.Behaviors
Assembly: Sartorius.SAF.Presentation.dll
Syntax
public class TextChangedCommandBehavior : CommandBehaviorBase<TextBox>

Constructors

View Source

TextChangedCommandBehavior(TextBox)

Initializes a new instance of the TextChangedCommandBehavior class.

Declaration
public TextChangedCommandBehavior(TextBox element)
Parameters
Type Name Description
TextBox element

Fields

View Source

CommandProperty

Command to execute on click event.

Declaration
public static readonly DependencyProperty CommandProperty
Field Value
Type Description
DependencyProperty

Methods

View Source

GetCommand(DependencyObject)

Retrieves the ICommand attached to the TextBox.

Declaration
public static ICommand GetCommand(DependencyObject dependencyObject)
Parameters
Type Name Description
DependencyObject dependencyObject

TextBox or PasswordBox containing the Command dependency property

Returns
Type Description
ICommand

The value of the command attached

View Source

SetCommand(DependencyObject, ICommand)

Sets the ICommand to execute on the click event.

Declaration
public static void SetCommand(DependencyObject dependencyObject, ICommand command)
Parameters
Type Name Description
DependencyObject dependencyObject

A dependency object to attach command

ICommand command

Command to attach

Extension Methods

CollectionExtensions.AddRange<T, TCollection>(TCollection, IEnumerable<T>)
SerializableObjectCloneExtension.Clone<T>(T)
  • View Source
Back to top Generated by DocFX