Show / Hide Table of Contents

Class MefRegionBehaviorFactory

Exports the RegionBehaviorFactory using the Managed Extensibility Framework (MEF).

Inheritance
object
RegionBehaviorFactory
MefRegionBehaviorFactory
Implements
IRegionBehaviorFactory
IEnumerable<string>
IEnumerable
RegionBehaviorFactory.AddIfMissing(string, Type)
RegionBehaviorFactory.ContainsKey(string)
RegionBehaviorFactory.CreateFromKey(string)
RegionBehaviorFactory.GetEnumerator()
object.Equals(object)
object.Equals(object, object)
object.GetHashCode()
object.GetType()
object.MemberwiseClone()
object.ReferenceEquals(object, object)
object.ToString()
Namespace: Sartorius.SAF.Presentation.MefExtensions
Assembly: Sartorius.SAF.Presentation.dll
Syntax
[Export(typeof(IRegionBehaviorFactory))]
[PartCreationPolicy(CreationPolicy.Shared)]
public class MefRegionBehaviorFactory : RegionBehaviorFactory, IRegionBehaviorFactory, IEnumerable<string>, IEnumerable
Remarks

This allows the MefBootstrapper to provide this class as a default implementation. If another implementation is found, this export will not be used.

Constructors

View Source

MefRegionBehaviorFactory(IServiceLocator)

Initializes a new instance of the MefRegionBehaviorFactory class.

Declaration
[ImportingConstructor]
public MefRegionBehaviorFactory(IServiceLocator serviceLocator)
Parameters
Type Name Description
IServiceLocator serviceLocator

CommonServiceLocator.IServiceLocator used to create the instance of the behavior from its Type.

Implements

IRegionBehaviorFactory
IEnumerable<T>
IEnumerable

Extension Methods

CollectionExtensions.AddRange<T, TCollection>(TCollection, IEnumerable<T>)
SerializableObjectCloneExtension.Clone<T>(T)
  • View Source
Back to top Generated by DocFX