Classes
Application
Encapsulates a Windows Presentation Foundation application.
ApplicationBootstrapper
Bootstrapper implementation for a WPF application.
ApplicationController
Is responsible for controlling application related actions.
ApplicationExceptionHandlingFacade
ExceptionHandling Facade for WPF applications.
BindingValueProvider
Provides binding to connect to the properties of a target object.
DispatcherWindow
Interaction logic for Window1.xaml
IdleTracker
Defines a tracker to track the idle time of the system.
Login
Provides information about the login process.
RoutedCommands
Provides functionality for binding CommandBindings and basic routed commands.
SpanExtensions
Provides extensions for Spans.
UserActivityMonitor
Implements the functionality for watcher of user activity. User is not active if it in given time interval don't move a mouse or type any key on keyboard. The extern timer can check if the user was active using the method WasUserActive().
Interfaces
IApplicationController
Defines methods to execute application related tasks.