Class MefDelayedRegionCreationBehavior
Exports the DelayedRegionCreationBehavior using the Managed Extensibility Framework (MEF).
Namespace: Sartorius.SAF.Presentation.MefExtensions
Assembly: Sartorius.SAF.Presentation.dll
Syntax
[Export(typeof(DelayedRegionCreationBehavior))]
[PartCreationPolicy(CreationPolicy.NonShared)]
public class MefDelayedRegionCreationBehavior : DelayedRegionCreationBehavior
Remarks
This allows the MefBootstrapper to provide this class as a default implementation. If another implementation is found, this export will not be used.
Constructors
View SourceMefDelayedRegionCreationBehavior(RegionAdapterMappings)
Initializes a new instance of the MefDelayedRegionCreationBehavior class.
Declaration
[ImportingConstructor]
public MefDelayedRegionCreationBehavior(RegionAdapterMappings regionAdapterMappings)
Parameters
| Type | Name | Description |
|---|---|---|
| RegionAdapterMappings | regionAdapterMappings | The region adapter mappings, that are used to find the correct adapter for
a given controltype. The controltype is determined by the |