Class OverlayArguments
Arguments for the overlay effect
Namespace: Sartorius.SAF.Presentation.Controls
Assembly: Sartorius.SAF.Presentation.Controls.dll
Syntax
public class OverlayArguments
Constructors
View SourceOverlayArguments()
Initializes a new empty instance of the OverlayArguments class.
Declaration
public OverlayArguments()
OverlayArguments(IEnumerable<FrameworkElement>)
Initializes a new instance of the OverlayArguments class with the specified excluded elements.
Declaration
public OverlayArguments(IEnumerable<FrameworkElement> excludedElements)
Parameters
| Type | Name | Description |
|---|---|---|
| IEnumerable<FrameworkElement> | excludedElements | The excluded elements. |
OverlayArguments(FrameworkElement)
Initializes a new instance of the OverlayArguments class that use the specified source reference to only overlay the source window.
Declaration
public OverlayArguments(FrameworkElement sourceReference)
Parameters
| Type | Name | Description |
|---|---|---|
| FrameworkElement | sourceReference | The source reference. |
OverlayArguments(FrameworkElement, IEnumerable<FrameworkElement>)
Initializes a new instance of the OverlayArguments class that use the specified source reference to only overlay the source window and excludes the specified excluded elements.
Declaration
public OverlayArguments(FrameworkElement sourceReference, IEnumerable<FrameworkElement> excludedElements)
Parameters
| Type | Name | Description |
|---|---|---|
| FrameworkElement | sourceReference | The source reference. |
| IEnumerable<FrameworkElement> | excludedElements | The excluded elements. |
Properties
View SourceExcludedElements
Gets the excluded elements.
Declaration
public ICollection<FrameworkElement> ExcludedElements { get; }
Property Value
| Type | Description |
|---|---|
| ICollection<FrameworkElement> | The excluded elements. |
Remarks
These elements will not be overlaid.
Force
Gets or sets a value indicating whether this OverlayArguments is forcing overlay over windows that do not allow an overlay.
Declaration
public bool Force { get; set; }
Property Value
| Type | Description |
|---|---|
| bool |
|
SourceReference
Gets or sets the source reference.
Declaration
public FrameworkElement SourceReference { get; set; }
Property Value
| Type | Description |
|---|---|
| FrameworkElement |
Remarks
This element is used to find the source window when Type is set to SourceWindow.
Type
Gets or sets the type of overlay.
Declaration
public OverlayType Type { get; set; }
Property Value
| Type | Description |
|---|---|
| OverlayType | The type of overlay. |
Remarks
When this is set to SourceWindow the SourceReference is used to find the source window to overlay.