Interface IOverlayEffect
Defines methods to apply overlay effects to windows.
Namespace: Sartorius.SAF.Presentation.Controls
Assembly: Sartorius.SAF.Presentation.Controls.dll
Syntax
public interface IOverlayEffect
Examples
The following example illustrates how to import the IOverlayEffect implementation.
The following example illustrates how to use the IOverlayEffect on all overlay-able windows.
The following example illustrates how to use the IOverlayEffect on all overlay-able windows but spare a single control.
The following example illustrates how to prevent a window from being overlaid by using the IsAllowedProperty.
<Window x:Class="ExcludedFromOverlay.MainWindow"
xmlns="http://schemas.microsoft.com/winfx/2006/xaml/presentation"
xmlns:x="http://schemas.microsoft.com/winfx/2006/xaml"
xmlns:d="http://schemas.microsoft.com/expression/blend/2008"
xmlns:mc="http://schemas.openxmlformats.org/markup-compatibility/2006"
xmlns:SAF="http://www.sartorius.com/SAF"
SAF:OverlayEffect.IsAllowed="False"
mc:Ignorable="d"
Title="Main Window" Height="300" Width="300">
<Grid>
<!-- content of window -->
</Grid>
</Window>
The following example shows how a style can manipulate the layout of a control when it is overlaid by an OverlayEffect.
<Style x:Key="DataGridStyle" TargetType="DataGrid">
<Style.Triggers>
<Trigger Property="SAF:OverlayEffect.IsOverlayed" Value="True">
<Setter Property="IsEnabled" Value="False" />
<Setter Property="CellStyle" Value="{StaticResource OverlayedCellStyle}" />
</Trigger>
</Style.Triggers>
</Style>
Methods
View SourceApply()
Applies an overlay effect to all application windows that don't have an overlay effect yet.
Declaration
IDisposable Apply()
Returns
| Type | Description |
|---|---|
| IDisposable | An instance of IDisposable that removes the effect on dispose. |
Remarks
Windows that have OverlayEffect.IsAllowed set to false will not get overlaid.
Apply(OverlayArguments)
Applies an overlay according to the specified OverlayArguments.
Declaration
IDisposable Apply(OverlayArguments arguments)
Parameters
| Type | Name | Description |
|---|---|---|
| OverlayArguments | arguments | The OverlayArguments that specify the scope of the overlay. |
Returns
| Type | Description |
|---|---|
| IDisposable | An instance of IDisposable that removes the effect on dispose. |
Remarks
In MVVM scenarios consider to use the OverlayEffectTriggerBehavior.