Class SerializationContext
This context can provide a custom SerilizationBinder to the legacy binary serialization.
Namespace: Sartorius.SAF.Serialization
Assembly: Sartorius.SAF.dll
Syntax
public class SerializationContext
Remarks
Generally you don't need to use this. It is used internally by SettingInfo when setting the CustomSerializationBinder.
Properties
View SourceBinder
Gets or set the working directory for the debug output files
Declaration
public SerializationBinder Binder { get; }
Property Value
| Type | Description |
|---|---|
| SerializationBinder |
Current
Gets the current debug context
Declaration
public static SerializationContext Current { get; }
Property Value
| Type | Description |
|---|---|
| SerializationContext |
Methods
View SourceUseContext(SerializationBinder)
Create a new serialization context using the specified SerializationBinder.
Declaration
public static IDisposable UseContext(SerializationBinder binder)
Parameters
| Type | Name | Description |
|---|---|---|
| SerializationBinder | binder |
Returns
| Type | Description |
|---|---|
| IDisposable | An IDisposable that defines the lifetime of the serialization context. |