Show / Hide Table of Contents

Class MefItemsControlRegionAdapter

Exports the ItemsControlRegionAdapter using the Managed Extensibility Framework (MEF).

Inheritance
object
RegionAdapterBase<ItemsControl>
ItemsControlRegionAdapter
MefItemsControlRegionAdapter
Implements
IRegionAdapter
ItemsControlRegionAdapter.Adapt(IRegion, ItemsControl)
ItemsControlRegionAdapter.CreateRegion()
RegionAdapterBase<ItemsControl>.Initialize(ItemsControl, string)
RegionAdapterBase<ItemsControl>.RegionBehaviorFactory
RegionAdapterBase<ItemsControl>.AttachBehaviors(IRegion, ItemsControl)
RegionAdapterBase<ItemsControl>.AttachDefaultBehaviors(IRegion, ItemsControl)
object.Equals(object)
object.Equals(object, object)
object.GetHashCode()
object.GetType()
object.MemberwiseClone()
object.ReferenceEquals(object, object)
object.ToString()
Namespace: Sartorius.SAF.Presentation.MefExtensions
Assembly: Sartorius.SAF.Presentation.dll
Syntax
[Export(typeof(ItemsControlRegionAdapter))]
[PartCreationPolicy(CreationPolicy.Shared)]
public class MefItemsControlRegionAdapter : ItemsControlRegionAdapter, IRegionAdapter
Remarks

This allows the MefBootstrapper to provide this class as a default implementation. If another implementation is found, this export will not be used.

Constructors

View Source

MefItemsControlRegionAdapter(IRegionBehaviorFactory)

Initializes a new instance of the MefItemsControlRegionAdapter class.

Declaration
[ImportingConstructor]
public MefItemsControlRegionAdapter(IRegionBehaviorFactory regionBehaviorFactory)
Parameters
Type Name Description
IRegionBehaviorFactory regionBehaviorFactory

The factory used to create the region behaviors to attach to the created regions.

Implements

IRegionAdapter

Extension Methods

CollectionExtensions.AddRange<T, TCollection>(TCollection, IEnumerable<T>)
SerializableObjectCloneExtension.Clone<T>(T)
  • View Source
Back to top Generated by DocFX