Show / Hide Table of Contents

Class DynamicObjectExtension

Can be used to create dynamic objects via markup. This can be used to create data-bound objects purely from Markup. E.g. for the ComboBoxItemDisplayBehavior.EmptyItem.

Inheritance
object
MarkupExtension
DynamicObjectExtension
object.Equals(object)
object.Equals(object, object)
object.GetHashCode()
object.GetType()
object.MemberwiseClone()
object.ReferenceEquals(object, object)
object.ToString()
Namespace: Sartorius.SAF.Presentation.Extensions
Assembly: Sartorius.SAF.Presentation.dll
Syntax
public class DynamicObjectExtension : MarkupExtension
Examples

The following XAML-markup creates an dynamic object with the signature below.

<SAF:DynamicObject x:Key="DynamicEmptyItem">
    <SAF:DynamicObject.Members>
        <system:String x:Key="Name">Empty Dynamic Item</system:String>
        <system:Int32 x:Key="Value">-1</system:Int32>
    </SAF:DynamicObject.Members>
</SAF:DynamicObject>
</code>
<code language="C#">
public class DynamicObject
{
    public string Name { get; set; }
    public int Value { get; set; }
}

Constructors

View Source

DynamicObjectExtension()

Creates a new Instance of DynamicObjectExtension

Declaration
public DynamicObjectExtension()

Properties

View Source

MemberName

Declaration
public string MemberName { get; set; }
Property Value
Type Description
string
View Source

MemberValue

Declaration
public object MemberValue { get; set; }
Property Value
Type Description
object
View Source

Members

Declaration
public Dictionary<string, object> Members { get; set; }
Property Value
Type Description
Dictionary<string, object>

Methods

View Source

ProvideValue(IServiceProvider)

When implemented in a derived class, returns an object that is provided as the value of the target property for this markup extension.

Declaration
public override object ProvideValue(IServiceProvider serviceProvider)
Parameters
Type Name Description
IServiceProvider serviceProvider

A service provider helper that can provide services for the markup extension.

Returns
Type Description
object

The object value to set on the property where the extension is applied.

Overrides
MarkupExtension.ProvideValue(IServiceProvider)

Extension Methods

CollectionExtensions.AddRange<T, TCollection>(TCollection, IEnumerable<T>)
SerializableObjectCloneExtension.Clone<T>(T)
  • View Source
Back to top Generated by DocFX