Show / Hide Table of Contents

Class WizardDialog

Invokes a dialog that displays a Wizard control.

Inheritance
object
WizardDialog
Implements
IWizardDialog
object.Equals(object)
object.Equals(object, object)
object.GetHashCode()
object.GetType()
object.MemberwiseClone()
object.ReferenceEquals(object, object)
object.ToString()
Namespace: Sartorius.SAF.Presentation.Controls
Assembly: Sartorius.SAF.Presentation.Controls.dll
Syntax
[Export(typeof(IWizardDialog))]
[PartCreationPolicy(CreationPolicy.NonShared)]
public class WizardDialog : IWizardDialog
Remarks

The wizard dialog should be imported by MEF using IWizardDialog.

For a detailed description how to create a wizard (which is used as content of this dialog), please see the documentation of the Wizard custom control.

See IWizardDialog for code examples.

Constructors

View Source

WizardDialog(ExportFactory<IContentDialog>)

Creates a new instance of the WizardDialog class.

Declaration
[ImportingConstructor]
public WizardDialog(ExportFactory<IContentDialog> contentDialogExportFactory)
Parameters
Type Name Description
ExportFactory<IContentDialog> contentDialogExportFactory

A factory to get instances of the IContentDialog.

Methods

View Source

Show(WizardDialogArgs)

Shows a message content that visualizes the information of the contentArgs.

Declaration
public void Show(WizardDialogArgs wizardDialogArgs)
Parameters
Type Name Description
WizardDialogArgs wizardDialogArgs

Definition of the information shown in the content dialog.

Remarks

See WizardDialog for remarks and code examples.

View Source

Show<TResult>(WizardDialogArgs)

Shows a dialog with the wizard defined in the wizardDialogArgs.

Declaration
public TResult Show<TResult>(WizardDialogArgs wizardDialogArgs)
Parameters
Type Name Description
WizardDialogArgs wizardDialogArgs

The WizardDialogArgs.

Returns
Type Description
TResult

The result.

Type Parameters
Name Description
TResult

the Type of the result.

Remarks

See WizardDialog for remarks and code examples.

Implements

IWizardDialog

Extension Methods

CollectionExtensions.AddRange<T, TCollection>(TCollection, IEnumerable<T>)
SerializableObjectCloneExtension.Clone<T>(T)
  • View Source
Back to top Generated by DocFX