Enum IconResourceKey
Defines keys for icon resources. The resources are styles for a ContentControl.
Namespace: Sartorius.SAF.Presentation.Controls.Resources
Assembly: Sartorius.SAF.Presentation.Controls.dll
Syntax
public enum IconResourceKey
Remarks
See documentation for each key whether the icon is available as vector graphic or bitmap. For vector based icons a default size is given but you can resize them as needed.
Fields
| Name | Description |
|---|---|
| Add | Icon for add command. |
| AddBookmark | Icon for a command that adds a bookmark. |
| AddComment | Icon for a command adding a comment. |
| Alert | A marker for an alert. |
| AlertHigh | High Alarm (values exceed e defined limit: High-Limit) |
| AlertHighHigh | High High Alarm (values exceed a defined limit: High-High-Limit) |
| AlertLow | Low Alarm (values fall below a defined limit: Low-Limit) |
| AlertLowLow | Low Low Alarm (values fall below a defined limit: Low-Low-Limit) |
| AlertStateOutOfService | Icon for out-of-service alert state. |
| AlertStateShelved | Icon for shelved alert state.# |
| AlertsAcknowledged | Icon for acknowledged alerts. |
| AlertsOutOfService | Icon for out-of-service alerts. |
| AlertsShelved | Icon for shelved alerts. |
| AlignLabelBottom | Icon for a command that aligns labels in a y-axis at the below tick marks. |
| AlignLabelHorizontal | Icon for a command that aligns labels in a y-axis horizontally (the label text will be written from left to right). |
| AlignLabelTop | Icon for a command that aligns labels in a y-axis at the top of tick marks. |
| AlignLabelVertical | Icon for a command that aligns labels in a y-axis vertically (the label text will be written from bottom to top). |
| AssignUser | Icon that represents the assignment of a user. |
| AutomaticRefresh | Icon for automatic refresh |
| Backspace | Icon for backspace |
| Backward | Icon for backwards navigation. |
| BatchStateIndicator | Icon for a indicator representing the batch state. |
| Bell | Icon that represents a bell. |
| BellStruckthrough | Icon that represents a bell which is struckthrough. |
| Bookmark | Icon for a bookmark. |
| Brackets | Icon for brackets |
| Browse | Icon for a browse command. |
| CertificateState | Icon for a command that opens a flyout for certificate state. |
| Check | Check icon for indicating selected items in multi select. |
| Checked | Icon for checked state. |
| Circle | Icon for a round marker. |
| Close | Icon for a close command. |
| CloseBranch | Icon for closing a treeview branch. |
| CloseMultimonitoring | Icon for a command that closes multi monitoring. |
| Cogwheel | Icon for a cogwheel. |
| Comment | Icon for a comment marker |
| Confirm | Icon for confirm command. |
| ConfirmComment | Icon for a command confirming/saving a comment. |
| ControlModeAuto | Icon for automatic control. |
| ControlModeCalculated | Icon for a calculated variable. |
| ControlModeCascade | Icon representing a cascaded control of a variable. |
| ControlModeLocal | Icon for local control (no remote control, control is local to the unit). |
| ControlModeManually | Icon for manual control. |
| ControlModeOff | Icon for disabled control. |
| ControlModeProfile | Icon for control by a predefined profile. |
| ControlModeRemote | Icon for remote control. |
| Copy | Icon for a copy command. |
| Cut | Icon that represents a cut action. |
| Delete | Icon for a delete command. |
| DeleteBookmark | Icon for a command that deletes a bookmark. |
| Details | Icon for a command that shows details. |
| Diamond | Icon for a diamond, |
| DownloadComplete | Icon for a completed download. |
| DownloadUpdate | Icon for a command that downloads updates. |
| Edit | Icon for edit command. |
| EditComment | Icon for a command editing a comment. |
| Error | Icon representing a system error. |
| ErrorProcess | Icon representing a process error. |
| Ethernet | Icon for interface type: Ethernet |
| EthernetB | Icon for interface type: Ethernet |
| Export | Icon for a export command. |
| ExtendDialogHorizontal | Icon for a command that shows an extended area in a dialog. |
| ExternalLink | Icon that represents an external link or opening with an external program. |
| FatalError | Icon representing a fatal error. |
| Favourite | Icon for a command that selects a favourite. |
| Filtered | Icon representing a set filter. |
| Finish | Icon representing a finish. |
| Finished | Icon for a finished marker (e.g. for process end). |
| FitToMaxHorizontal | Icon to fit a range to maximum horizontally. |
| FitToMaxVertical | Icon to fit a range to maximum vertically. |
| FlyoutArrow | Icon for a command that opens a flyout. |
| Forward | Icon for forward navigation. |
| Fullscreen | Icon for a fullscreen command. |
| HasAttachment | Icon for an existing attachment. |
| Hashtag | A hashtag icon. |
| Help | Icon for a command to open help. |
| HelpHome | Icon for a command returing to the home screen. |
| HelpNotification | Icon for help notification. |
| HideFilterArea | Icon to hide the filter area. |
| Import | Icon for a import command. |
| Index | Icon for the index (overview of help topics). |
| Information | Icon representing information. |
| Input | Icon that represents a user input. |
| Instrument | Icon that represents an instrument (depicted by a Sartorius lens). |
| Invert | Icon for a command that inverts checkboxes. |
| Linked | Item for a command that links timelines. |
| ListAccess | Icon for a command that opens list access. |
| LoadGroup | Icon for a command that loads a group. |
| LoadTemplate | Icon for a command that loads a template. |
| LockAccount | Icon for a command that locks an account |
| Login | Icon that represents a login. |
| Logout | Icon for a logout command. |
| MarkAsRead | Icon for a command that marks items as read. |
| MarkAsUnread | Icon for a command that marks items as unread. |
| Maximize | Icon for a command to maximize a window. |
| Minimize | Icon for a minimize command. |
| ModifiedValueEdit | Icon representing a currently edited value. |
| ModifiedValueList | Icon representing an edited value in a list. |
| More | Icon that represents a more (...) action. |
| Multimonitoring | Icon for a command that maximizes the current content to a further display. |
| MultipleAttachments | Icon for an attachment command that opens a flyout. |
| Next | Icon for next |
| Normalize | Icon for a command to normalize a window. |
| NotEditable | Icon for a not-editable state. |
| OPC | Icon for interface type: OPC |
| OneLevelBack | Icon for a command that moves one level back. |
| Open | Icon for an open command. |
| OpenAttachment | Icon that represents opening an attachment. |
| OpenBranch | Icon for opening a treeview branch. |
| OpenDialog | Icon for a command that opens a dialog. |
| OrientationLandscape | Icon for landscape orientation. |
| OrientationPortrait | Icon for portrait orientation. |
| Output | Icon for the output of a variable. |
| ParallelBranch | Icon that represents a parallel branch. |
| Parameter | Icon for a parameter. |
| Paste | Icon that represents a paste action. |
| Pause | Icon that represents a pause action. |
| Phase | Icon that represents a phase. |
| Play | Icon that represents a play action. |
| PlayButton | Icon that represents a play button. |
| Previous | Icon for previous |
Icon for a print command. |
|
| PrintAll | Icon for a print all command. |
| ProcessTime | Icon for the time passed since process start. |
| Profile | Icon for a profile. |
| Question | Icon representing a question. |
| REST | Icon for interface type: REST |
| RS232 | Icon for interface type: RS232 |
| RS422 | Icon for interface type: RS 422 |
| RadioButton | Icon for indicating selected item in single select. |
| Random | Icon for random value |
| Rect | Icon for a rectangular marker. |
| Redo | Icon that represents a redo action. |
| Refresh | Icon for a refresh command. |
| RemarkPositionBottomLeft | Icon for position of a remark in the bottom left corner. |
| RemarkPositionBottomRight | Icon for position of a remark in the bottom right corner. |
| RemarkPositionTopLeft | Icon for position of a remark in the top left corner. |
| RemarkPositionTopRight | Icon for position of a remark in the top right corner. |
| Reminder | Icon for a reminder. |
| RemoteCalculated | Icon for a mode remote calculated. |
| Remove | Icon for remove command. |
| RemoveUser | Icon that represents the removal of a user. |
| Replace | Icon for a replace command. |
| Report | Icon for a report. |
| ReportConfig | Icon for report configuration. |
| Reset | Icon for reset command. |
| Root | Icon for mathematical root sign |
| SaveTemplate | Icon for a command that saves a template. |
| SearchResults | Icon for search results. |
| SelectAll | Icon for a command that selects all checkboxes. |
| SelectNone | Icon for a command that deselects all checkboxes. |
| SelectSearchCriteria | Icon for a command that lets the user select the search criteria. |
| SendAsEmail | Icon for a command that sends content by email. |
| Sequence | Icon for a sequence. |
| Setpoint | Icon for the setpoint of a variable. |
| SetpointIndicatorLeft | Icon for a setpoint indicator to the left. |
| SetpointIndicatorRight | Icon for a setpoint indicator to the right. |
| Settings | Icon for settings. |
| ShowDetails | Icon for a command that shows details. |
| ShowFilterArea | Icon for a command that shows the filter area. |
| Shutdown | Icon for a shutdown command. |
| Silence | Icon for silence |
| Simulation | Schnittstelle Typ: Simulation |
| SingleAttachment | Icon for an attachment command. If you want to just visualize the existence of an attachment without the need for a command use HasAttachment. |
| Skip | Icon that represents a skip action. |
| SortAscending | Icon for sorting ascending. |
| SortBy | Icon to select a sort criteria. |
| SortDescending | Icon to sort descending. |
| Stop | Icon that represents a stop action. |
| StopButton | Icon that represents a stop button. |
| Stopwatch | Icon for a stopwatch. |
| Suppress | Icon for suppress |
| Sync | Icon for a sync command. |
| Target | Icon for a target (e.g. a setpoint). |
| TestConnection | Icon for a command that tests a connection (e.g. to a device). |
| TimeReset | Icon that represents a reset of time. |
| Tooltip | Icon for a tooltip or message. |
| Transition | Icon that represents a transition. |
| Transitions | Icon that represents many transitions. |
| TriangleDown | Icon for a triangular marker pointing upwards. |
| TriangleUp | Icon for a triangular marker pointing downwards. |
| UnLinked | Icon for a command that undoes linking. |
| Unchecked | Icon for unchecked state. |
| Undo | Icon that represents an undo action. |
| UndoSilence | Icon for undo silence |
| Unit | Icon for a unit generic unit. |
| UnitType05 | Icon for a unit (0,5L) |
| UnitType1 | Icon for a unit (1L) |
| UnitType10 | Icon for a unit (10L) |
| UnitType100 | Icon for a unit (100L) |
| UnitType2 | Icon for a unit (2L) |
| UnitType20 | Icon for a unit (20L) |
| UnitType200 | Icon for a unit (200L) |
| UnitType2500 | Icon for a unit (2500L) |
| UnitType30 | Icon for a unit (30L) |
| UnitType5 | Icon for a unit (5L) |
| UnitType50 | Icon for a unit (50L) |
| UnitType600 | Icon for a unit (600L) |
| Unknown | Icon for a mode remote calculated. |
| UnselectedCheckbox | Icon for the readonly state of an unselected checkbox. |
| User | Icon that represents a user. |
| UserInteraction | Icon for a user interaction. |
| UserSettings | Icon for a command that opens user settings. |
| ValidateEntry | Icon for a validation command. |
| Warning | Icon representing a warning. |
| WarningRed | Icon that represents warning. |
| WarningSign | Icon that represents a warning sign. |
| WorkingIndicatorGrey | Loading indicator for an indeterminate loading time. |
| WorkingIndicatorWhite | Loading indicator for an indeterminate loading time. |
| ZoomIn | Icon for zooming in |