Show / Hide Table of Contents

Classes

BrushExtension

Defines a MarkupExtension to provide a Brush based on the given BrushResourceKey.

IconExtension

Defines a MarkupExtension to provide a Style for a ContentControl representing an icon based on the given IconResourceKey or a ContentControl if the value is provided for the ContentProperty.

ModuleIconExtension

Defines a MarkupExtension to provide a Style for a ContentControl representing an icon based on the given ModuleIconResourceKey or a ContentControl if the value is provided for the ContentProperty.

StyleExtension

Defines a MarkupExtension to provide a Style based on the given StyleResourceKey.

WpfResourceMarkupExtensionBase<TResource, TResourceKey>

Defines a base class to provide wpf resources via markup extension.

Back to top Generated by DocFX