Show / Hide Table of Contents

Class FileDialogArgs

Encapsulates arguments for the IFileDialog.

Inheritance
object
FileDialogArgs
object.Equals(object)
object.Equals(object, object)
object.GetHashCode()
object.GetType()
object.MemberwiseClone()
object.ReferenceEquals(object, object)
object.ToString()
Namespace: Sartorius.SAF.Presentation.Controls
Assembly: Sartorius.SAF.Presentation.Controls.dll
Syntax
public class FileDialogArgs

Constructors

View Source

FileDialogArgs()

Creates a new instance of the FileDialogArgs class.

Declaration
public FileDialogArgs()
View Source

FileDialogArgs(FileType)

Creates a new instance of the FileDialogArgs class.

Declaration
public FileDialogArgs(FileType fileType)
Parameters
Type Name Description
FileType fileType

The supported FileType.

Examples
var fileDialogArgs = new FileDialogArgs(FileType.Csv | FileType.Access);

Properties

View Source

AddExtension

Indicates whether to add the extension by default.

Declaration
public bool AddExtension { get; set; }
Property Value
Type Description
bool
View Source

DefaultExtension

Gets or sets the default file name extension.

Declaration
public string DefaultExtension { get; set; }
Property Value
Type Description
string
View Source

DefaultFileName

Gets or sets the file name that should be used initially in the file dialog box.

Declaration
public string DefaultFileName { get; set; }
Property Value
Type Description
string
Remarks

If this is null or Empty the file name box will be empty when the dialog box is opened.

This can be a fully qualified file name. The current implementation sets the InitialDirectory accordingly if it has not been explicitly set. If the InitialDirectory is set to a different directory the given InitialDirectory will shown in the FileView but the DefaultFileName will be set to the given fully qualified name. You can not rely on this behavior in future implementations.

View Source

FileType

The supported FileType.

Declaration
public FileType FileType { get; set; }
Property Value
Type Description
FileType
View Source

Filter

Gets or sets the value that is used to filter the file selection by extension.

Declaration
public string Filter { get; set; }
Property Value
Type Description
string
View Source

InitialDirectory

Gets or sets the initial directory.

Declaration
public string InitialDirectory { get; set; }
Property Value
Type Description
string
Remarks

The initial directory must be valid path. Trying to set an invalid path will ignore the value completely.

View Source

MultiSelect

Indicates whether the IFileDialog allows multi selection.

Declaration
public bool MultiSelect { get; set; }
Property Value
Type Description
bool

Extension Methods

CollectionExtensions.AddRange<T, TCollection>(TCollection, IEnumerable<T>)
SerializableObjectCloneExtension.Clone<T>(T)
  • View Source
Back to top Generated by DocFX