Class ErrorRoutedEventArgs
Provides data about an exception that occured during an operation.
Inheritance
System.Object
ErrorRoutedEventArgs
Namespace: Sartorius.SAF.Presentation.Controls
Assembly: Sartorius.SAF.Presentation.Controls.Pdf_hpsftrbd_wpftmp.dll
Syntax
public class ErrorRoutedEventArgs : RoutedEventArgs
Constructors
View SourceErrorRoutedEventArgs(Exception)
Initializes a new instance of the ErrorRoutedEventArgs class with the specified exception.
Declaration
public ErrorRoutedEventArgs(Exception error)
Parameters
| Type | Name | Description |
|---|---|---|
| Exception | error | The error that has occured. |
ErrorRoutedEventArgs(String, Exception)
Initializes a new instance of the ErrorRoutedEventArgs class with the specified command name and exception.
Declaration
public ErrorRoutedEventArgs(String commandName, Exception error)
Parameters
| Type | Name | Description |
|---|---|---|
| String | commandName | The name of the command during which the error occured. |
| Exception | error | The error that has occured. |
Properties
View SourceCommandName
Gets the name of the command during which the error occured.
Declaration
public String CommandName { get; }
Property Value
| Type | Description |
|---|---|
| String |
Error
Gets the
Declaration
public Exception Error { get; }
Property Value
| Type | Description |
|---|---|
| Exception |
ErrorHandled
Gets or sets a value indicating if the error was handled by the subscriber.
Declaration
public Boolean ErrorHandled { get; set; }
Property Value
| Type | Description |
|---|---|
| Boolean |
Remarks
If this is not set to true by a subscriber, the exception will be thrown.