Class CompositeCommand
The CompositeCommand composes one or more ICommands.
Implements
Namespace: Sartorius.SAF.Presentation.Commands
Assembly: Sartorius.SAF.Presentation.dll
Syntax
public class CompositeCommand : ICommand
Constructors
View SourceCompositeCommand()
Initializes a new instance of CompositeCommand.
Declaration
public CompositeCommand()
CompositeCommand(bool)
Initializes a new instance of CompositeCommand.
Declaration
public CompositeCommand(bool monitorCommandActivity)
Parameters
| Type | Name | Description |
|---|---|---|
| bool | monitorCommandActivity | Indicates when the command activity is going to be monitored. |
Properties
View SourceRegisteredCommands
Gets the list of all the registered commands.
Declaration
public IList<ICommand> RegisteredCommands { get; }
Property Value
| Type | Description |
|---|---|
| IList<ICommand> | A list of registered commands. |
Remarks
This returns a copy of the commands subscribed to the CompositeCommand.
Methods
View SourceCanExecute(object)
Forwards CanExecute(object) to the registered commands and returns true if all of the commands return true.
Declaration
public virtual bool CanExecute(object parameter)
Parameters
| Type | Name | Description |
|---|---|---|
| object | parameter | Data used by the command. If the command does not require data to be passed, this object can be set to null. |
Returns
| Type | Description |
|---|---|
| bool |
Execute(object)
Forwards Execute(object) to the registered commands.
Declaration
public virtual void Execute(object parameter)
Parameters
| Type | Name | Description |
|---|---|---|
| object | parameter | Data used by the command. If the command does not require data to be passed, this object can be set to null. |
OnCanExecuteChanged()
Raises CanExecuteChanged on the UI thread so every command invoker can query CanExecute(object) to check if the CompositeCommand can execute.
Declaration
protected virtual void OnCanExecuteChanged()
RegisterCommand(ICommand)
Adds a command to the collection and signs up for the CanExecuteChanged event of it.
Declaration
public virtual void RegisterCommand(ICommand command)
Parameters
| Type | Name | Description |
|---|---|---|
| ICommand | command | The command to register. |
Remarks
If this command is set to monitor command activity, and command
implements the IActiveAware interface, this method will subscribe to its
IsActiveChanged event.
ShouldExecute(ICommand)
Evaluates if a command should execute.
Declaration
protected virtual bool ShouldExecute(ICommand command)
Parameters
| Type | Name | Description |
|---|---|---|
| ICommand | command | The command to evaluate. |
Returns
| Type | Description |
|---|---|
| bool | A bool value indicating whether the command should be used when evaluating CanExecute(object) and Execute(object). |
Remarks
If this command is set to monitor command activity, and command
implements the IActiveAware interface,
this method will return false if the command's IsActive
property is false; otherwise it always returns true.
UnregisterCommand(ICommand)
Removes a command from the collection and removes itself from the CanExecuteChanged event of it.
Declaration
public virtual void UnregisterCommand(ICommand command)
Parameters
| Type | Name | Description |
|---|---|---|
| ICommand | command | The command to unregistered. |
Events
View SourceCanExecuteChanged
Occurs when any of the registered commands raise CanExecuteChanged. You must keep a hard reference to the handler to avoid garbage collection and unexpected results. See remarks for more information.
Declaration
public event EventHandler CanExecuteChanged
Event Type
| Type | Description |
|---|---|
| EventHandler |
Remarks
When subscribing to the CanExecuteChanged event using code (not when binding using XAML) will need to keep a hard reference to the event handler. This is to prevent garbage collection of the event handler because the command implements the Weak Event pattern so it does not have a hard reference to this handler. An example implementation can be seen in the CompositeCommand and CommandBehaviorBase classes. In most scenarios, there is no reason to sign up to the CanExecuteChanged event directly, but if you do, you are responsible for maintaining the reference.
Examples
The following code holds a reference to the event handler. The myEventHandlerReference value should be stored in an instance member to avoid it from being garbage collected.
EventHandler myEventHandlerReference = new EventHandler(this.OnCanExecuteChanged);
command.CanExecuteChanged += myEventHandlerReference;