Class FeatureException
The exception that is thrown when the requested feature.
Implements
System.Runtime.Serialization.ISerializable
System.Exception.GetBaseException()
System.Exception.GetObjectData(System.Runtime.Serialization.SerializationInfo, System.Runtime.Serialization.StreamingContext)
System.Exception.GetType()
System.Exception.ToString()
System.Exception.Data
System.Exception.HelpLink
System.Exception.HResult
System.Exception.InnerException
System.Exception.Message
System.Exception.Source
System.Exception.StackTrace
System.Exception.TargetSite
System.Exception.SerializeObjectState
System.Object.Equals(System.Object)
System.Object.Equals(System.Object, System.Object)
System.Object.GetHashCode()
System.Object.MemberwiseClone()
System.Object.ReferenceEquals(System.Object, System.Object)
Namespace: Sartorius.SAF.Licensing.Revenera.Exceptions
Assembly: Sartorius.SAF.Licensing.Revenera.dll
Syntax
[Serializable]
public class FeatureException : LicenseException, ISerializable
Constructors
View SourceFeatureException()
Create a new instance of FeatureException class.
Declaration
public FeatureException()
FeatureException(SerializationInfo, StreamingContext)
Initializes a new instance of the FeatureException class with serialized data.
Declaration
protected FeatureException(SerializationInfo si, StreamingContext ctx)
Parameters
Type | Name | Description |
---|---|---|
System.Runtime.Serialization.SerializationInfo | si | The System.Runtime.Serialization.SerializationInfo that holds the serialized object data about the exception being thrown. |
System.Runtime.Serialization.StreamingContext | ctx | The System.Runtime.Serialization.StreamingContext that contains contextual information about the source or destination. |
FeatureException(String)
Initializes a new instance of the FeatureException class with a specified error message.
Declaration
public FeatureException(string message)
Parameters
Type | Name | Description |
---|---|---|
System.String | message | The error message that explains the reason for the exception. |
FeatureException(String, Exception)
Initializes a new instance of the FeatureException class with a specified error message.
Declaration
public FeatureException(string message, Exception innerException)
Parameters
Type | Name | Description |
---|---|---|
System.String | message | The error message that explains the reason for the exception. |
System.Exception | innerException | The inner exception. |
Implements
System.Runtime.Serialization.ISerializable