Show / Hide Table of Contents

Class LicenseException

Represents errors that can occur while working with licenses.

Inheritance
System.Object
System.Exception
LicenseException
ActivationKeyAlreadyUsedException
FeatureAlreadyExistsException
FeatureNotFoundException
InvalidActivationKeyException
InvalidHardwareIdException
InvalidLicenseException
InvalidLicenseFileException
LicenseFileAccessException
LicenseKeysException
LicenseTamperedException
SystemDateChangedException
Implements
System.Runtime.Serialization.ISerializable
System.Exception.GetBaseException()
System.Exception.GetObjectData(System.Runtime.Serialization.SerializationInfo, System.Runtime.Serialization.StreamingContext)
System.Exception.GetType()
System.Exception.ToString()
System.Exception.Data
System.Exception.HelpLink
System.Exception.HResult
System.Exception.InnerException
System.Exception.Message
System.Exception.Source
System.Exception.StackTrace
System.Exception.TargetSite
System.Exception.SerializeObjectState
System.Object.Equals(System.Object)
System.Object.Equals(System.Object, System.Object)
System.Object.GetHashCode()
System.Object.MemberwiseClone()
System.Object.ReferenceEquals(System.Object, System.Object)
Namespace: Sartorius.SAF.Licensing
Assembly: Sartorius.SAF.Licensing.dll
Syntax
[Serializable]
public class LicenseException : Exception, ISerializable

Constructors

View Source

LicenseException()

Initializes a new instance of the LicenseException class.

Declaration
public LicenseException()
View Source

LicenseException(SerializationInfo, StreamingContext)

Initializes a new instance of the LicenseException class with serialized data.

Declaration
protected LicenseException(SerializationInfo si, StreamingContext ctx)
Parameters
Type Name Description
System.Runtime.Serialization.SerializationInfo si

The System.Runtime.Serialization.SerializationInfo that holds the serialized object data about the exception being thrown.

System.Runtime.Serialization.StreamingContext ctx

The System.Runtime.Serialization.StreamingContext that contains contextual information about the source or destination.

View Source

LicenseException(String)

Initializes a new instance of the LicenseException class with a specified error message.

Declaration
public LicenseException(string message)
Parameters
Type Name Description
System.String message

The error message that explains the reason for the exception.

View Source

LicenseException(String, Exception)

Initializes a new instance of the LicenseException class with a specified error message and a reference to the inner exception that is the cause of this exception..

Declaration
public LicenseException(string message, Exception innerException)
Parameters
Type Name Description
System.String message

The error message that explains the reason for the exception.

System.Exception innerException

The exception that is the cause of the current exception, or a null reference if no inner exception is specified.

Implements

System.Runtime.Serialization.ISerializable

Extension Methods

CollectionExtensions.AddRange<T, TCollection>(TCollection, IEnumerable<T>)
ExceptionExtensions.GetRootException(Exception)
SerializableObjectCloneExtension.Clone<T>(T)
  • View Source
Back to top Generated by DocFX