Show / Hide Table of Contents

Class CustomHandledException

Represents an exception which has been created during custom handling of an unhandled exception.

Inheritance
object
Exception
CustomHandledException
Implements
ISerializable
Exception.GetBaseException()
Exception.GetType()
Exception.ToString()
Exception.Data
Exception.HelpLink
Exception.HResult
Exception.InnerException
Exception.Message
Exception.Source
Exception.StackTrace
Exception.TargetSite
Exception.SerializeObjectState
object.Equals(object)
object.Equals(object, object)
object.GetHashCode()
object.MemberwiseClone()
object.ReferenceEquals(object, object)
Namespace: Sartorius.SAF.ExceptionHandling
Assembly: Sartorius.SAF.dll
Syntax
[Serializable]
public class CustomHandledException : Exception, ISerializable

Constructors

View Source

CustomHandledException()

Create a new instance of CustomHandledException.

Declaration
public CustomHandledException()
View Source

CustomHandledException(string)

Create a new instance of CustomHandledException.

Declaration
public CustomHandledException(string message)
Parameters
Type Name Description
string message

The error message that explains the reason for the exception.

View Source

CustomHandledException(string, Exception)

Initializes a new instance of the CustomHandledException class.

Declaration
public CustomHandledException(string message, Exception innerException)
Parameters
Type Name Description
string message

The error message that explains the reason for the exception.

Exception innerException

The exception that is the cause of the current exception, or a null reference (Nothing in Visual Basic) if no inner exception is specified.

Implements

ISerializable

Extension Methods

CollectionExtensions.AddRange<T, TCollection>(TCollection, IEnumerable<T>)
SerializableObjectCloneExtension.Clone<T>(T)
ExceptionExtensions.GetRootException(Exception)
  • View Source
Back to top Generated by DocFX