Show / Hide Table of Contents

Classes

AutoPopulateRegionBehavior

Populates the target region with the views registered to it in the IRegionViewRegistry.

BindRegionContextToDependencyObjectBehavior

Defines a behavior that forwards the RegionContextProperty to the views in the region.

DelayedRegionCreationBehavior

Behavior that creates a new IRegion, when the control that will host the IRegion (see TargetElement) is added to the VisualTree. This behavior will use the RegionAdapterMappings class to find the right type of adapter to create the region. After the region is created, this behavior will detach.

RegionActiveAwareBehavior

Behavior that monitors a IRegion object and changes the value for the IsActive property when an object that implements IActiveAware gets added or removed from the collection.

RegionCreationException

Represents errors that occured during region creation.

RegionManagerRegistrationBehavior

Subscribes to a static event from the RegionManager in order to register the target IRegion in a IRegionManager when one is available on the host control by walking up the tree and finding a control whose RegionManagerProperty property is not null.

RegionMemberLifetimeBehavior

The RegionMemberLifetimeBehavior determines if items should be removed from the IRegion when they are deactivated.

SyncRegionContextWithHostBehavior

Behavior that synchronizes the Context property of a IRegion with the control that hosts the Region. It does this by setting the RegionContextProperty Dependency Property on the host control. This behavior allows the usage of two way databinding of the RegionContext from XAML.

Interfaces

IHostAwareRegionBehavior

Defines a IRegionBehavior that not allows extensible behaviors on regions which also interact with the target element that the IRegion is attached to.

Back to top Generated by DocFX