Show / Hide Table of Contents

Interface IApp

The entry point of the application.

Namespace: Sartorius.SAF.Presentation.Infrastructure
Assembly: Sartorius.SAF.Presentation.dll
Syntax
public interface IApp

Methods

View Source

CanClose()

Indicates whether the application can be closed.

Declaration
bool CanClose()
Returns
Type Description
bool

True if the application can be closed, otherwise false.

Remarks

This method is called when MainWindow is closing. When this method returns false, the Cancel property is set to true, which prevents closing the MainWindow.

View Source

Run()

Runs the application.

Declaration
void Run()
Remarks

This method is called after the bootstrapping process has been finished.

Extension Methods

CollectionExtensions.AddRange<T, TCollection>(TCollection, IEnumerable<T>)
SerializableObjectCloneExtension.Clone<T>(T)
  • View Source
Back to top Generated by DocFX