Show / Hide Table of Contents

Interface IAsyncDelegateCommand

Defines methods for an asynchronous delegate command.

ICommand.CanExecute(object)
ICommand.Execute(object)
ICommand.CanExecuteChanged
Namespace: Sartorius.SAF.Presentation.Commands
Assembly: Sartorius.SAF.Presentation.dll
Syntax
public interface IAsyncDelegateCommand : ICommand

Methods

View Source

CanExecute()

Defines the method that determines whether the command can execute in its current state.

Declaration
bool CanExecute()
Returns
Type Description
bool

true, if this command can be executed; otherwise, false.

View Source

Execute()

Defines the method to be called when the command is invoked.

Declaration
Task Execute()
Returns
Type Description
Task

The task object representing the asynchronous operation.

Extension Methods

CollectionExtensions.AddRange<T, TCollection>(TCollection, IEnumerable<T>)
SerializableObjectCloneExtension.Clone<T>(T)
  • View Source
Back to top Generated by DocFX