Enum LicenseFileToken
Specifies mirage license file tokens used to get or set license file values.
Namespace: Sartorius.SAF.Licensing.Mirage
Assembly: Sartorius.SAF.Licensing.Mirage.dll
Syntax
public enum LicenseFileToken
Fields
Name | Description |
---|---|
CPT | Use this token to get or set the active type of Copy Protection. |
CST | Use this token to get or set the customer's name. |
FID | Use this token to get the license ID of the license file. |
ICO | Use this token to get or set the installation code (8 digit code) the license file is bound to. |
LTG | Use this token to get or set the tag of the license file. |
MID | Use this token to get or set the main module ID. |
OEM | Use this token to get or set the manufacturer's name. |
SEL | Use this token to get or set the security level of the license file. |
VER | Use this token to get or set the application version of the license file. |
VSN | Use this token to get the version of the license file. |