Enum FeatureToken
Specifies mirage license feature tokens used to get or set license feature values.
Namespace: Sartorius.SAF.Licensing.Mirage
Assembly: Sartorius.SAF.Licensing.Mirage.dll
Syntax
public enum FeatureToken
Fields
Name | Description |
---|---|
ALW | Use this token to get or set a value indicating whether the feature is allowed. |
DMO | Use this token to get or set a value indicating whether the feature is in demo mode. |
DPC | Use this token to get or set the tolerance in percent that is allowed for a client to do an automatic validate at a concurrent user module. |
EXO | Use this token to get or set the date when the feature expires. |
KYS | Use this token to get all standard keys for that module, separated by semicolon, including hidden keys. |
LAM | Use this token to get the last activation date of a feature |
LTY | Use this token to get or set the license type of a feature |
MEO | Use this token to get or set the maximum expiration date. |
MOI | Use this token to get or set the module id of a feature. |
MON | Use this token to get or set the name of the specified module. |
MYS | Use this token to get all standard keys for that module, separated by semicolon. Hidden keys are displayed as *****. |
NOD | use this token to get the number of days the feature is valid. |
SAC | Use this token to get or set the ActivationState after copy protection is turned on (unlock). |
SNR | Use this token to get or set the serial number for the feature. |
TAG | Use this token to get or set the tag value of the feature. |
TLI | Use this token to get or set the total license count of feature. |
WST | Use this token to get or set the web activation value |