Classes
AccessRightExtensions
Defines extensions for the AccessRight class.
AssemblyExtensions
Extension methods for the Assembly class.
CollectionExtensions
Class that provides extension methods to Collection
DateTimeExtensions
Provides extension methods for DateTime.
DecimalExtensions
Extension methods for decimal.
DeferrableObservableCollectionExtensions
Extension methods for DeferrableObservableCollection<T>.
DoubleExtensions
Provides extension methods for double
EnumExtensions
Extension methods for Enum.
EnumerableExtensions
Extension methods for IEnumerable<T>.
EventHandlerExtensions
Provides extension methods for delegates
ExceptionExtensions
Class that provides extension methods for the Exception class. These extension methods provide a mechanism for developers to get more easily to the root cause of an exception, especially in combination with DI-containers such as Unity.
ExpressionFuncTExtensions
Extension methods for Expression<TDelegate> of Func<TResult> and Func<T, TResult>.
ListExtensions
Enhances the object list's
NotifyPropertyChangedExtensions
Extension method for INotifyPropertyChanged.
ObservableCollectionExtensions
Provides extension methods for ObservableCollection<T>s
PropertyHelper
Extension-Method for PropertyChanged. If you don't like to inherit from ModelBase, use this.
SerializableObjectCloneExtension
Reference Article http://www.codeproject.com/KB/tips/SerializedObjectCloner.aspx Provides a method for performing a deep copy of an object. Binary Serialization is used to perform the copy.
ServiceFactoryExtensions
Implements extensions for the IServiceFactory to call service methods asynchronously or synchronously .
StringExtensions
Class encapsulating extension for String class.